UF_PATH_cutcom_s
(view source)
Defined in: uf_path.h
Also known as:
UF_PATH_cutcom_t
Overview
Specify data for the CUTCOM/ post command.
Data Members
cutcom_mode
UF_PATH_cutcom_mode_t
plane_type
UF_PATH_plane_type_t
cutcom_on_status
UF_PATH_cutcom_on_t
cutcom_off_status
UF_PATH_cutcom_off_t
adjust_register
int
the register to use for
cutter compensation
full_cutcom_output
logical
a full cutcom command
is output if and only
if this flag is TRUE.
adjust_flag
logical
the adjust register is
output if and only if
this flag is TRUE.