UF_OPER_status_s (view source)
Defined in: uf_oper.h
Also known as:
- UF_OPER_status_t
- UF_OPER_status_p_t
Overview
Operation Status: for all bit fields if the bit == 0 then the condition
represented by that bit is FALSE, otherwise it is TRUE
Data Members
:1
unsigned int is_edited
:1
unsigned int toolpath_exists
:1
unsigned int toolpath_edited
:29
unsigned int open