UF_NXSM_mitre_cflange_data_s (view source)
Defined in: uf_nxsm_types.h
Also known as:
- UF_NXSM_mitre_cflange_data_t
- UF_NXSM_mitre_cflange_data_p_t
Overview
Data structure for Mitre cut
Mitre cut is essentially an end treatment to the contour flange feature, which shall
prevent merging/interference with the existing or newly placed features in sheet metal.
Sometimes without mitreing we would end up with merging the faces of the adjoining
contour flange features.
The mitre cut is optional, and can be done in two ways. Either ?Normal to thickness face?
or ?Normal to source face' which is same as 'Parallel to thickness face?.
Mitreing is provided at the start or end of contour flange or at both start and end of
contour flange.
Data Members
mitre_position
mitre_type_at_start
mitre_type_at_end
mitre_side_at_start
mitre_side_at_end
mitre_by_dist_or_angle_at_start
mitre_by_dist_or_angle_at_end
mitre_angle_at_start [ UF_MAX_EXP_BUFSIZE ]
char
mitre_angle_at_end [ UF_MAX_EXP_BUFSIZE ]
char
mitre_cut_type
close_corner_type
close_corner_dia [ UF_MAX_EXP_BUFSIZE ]
char
IG_NONE - no mitre(default) ,
IG_START - mitre at start,
IG_RIGHT - mitre at end,