UF_MOTION_point_curve_constraint_s
(view source)
Defined in: uf_motion_types.h
Also known as:
UF_MOTION_point_curve_constraint_t
Data Members
name [ UF_OBJ_NAME_BUFSIZE ]
char
The name of the point curve
constraint. If NULL, a default
name will be created.
num_curve_tags
int
The number of tags in the curve
tag array.
curve
tag_t *
The tags of the constraint
curves. All curves must be on
same link (or no link).
point
tag_t
The tag of the constrained point.
It cannot belong to the same link
as the curves. See uf_so.h for
smart point creation methods.
constraint. If NULL, a default
name will be created.