Smart point that defines the origin of the marker. Note that this object is currently not saved in the database with the marker, it is included here for future enhancement. However, it is used to extract the coordinates in lieu of the user manually supplying or determining the coordinates of the marker.
location [ 3 ]
double
Coordinates that define the location of the marker.
a default name will be created.