Smart point at the center of mass. If the mass properties are automatically calculated, this will be the same as the origin of the marker below. These origins can be different for user defined mass properties.
Internal marker that defines the origin and orientation of the inertia values. If the mass properties are automatically generated, the origin will be the same as the mass_center above and the orientation will be the principle axes.
mass
double
The mass of the link
products_of_inertia [ 6 ]
double
The products of inertia of the link in the following order: Ixx, Ixy, Ixz, Iyy, Iyz, Iyz
If the mass properties are automatically
calculated, this will be the same
as the origin of the marker below.
These origins can be different
for user defined mass properties.