The name of the function object. There is no automatic default naming, a new name must be input for creation of function.
definition
char * *
String of the function definition. Function string can contain standard math functions, Adams variables and functions, and derived functions of motion object results. It is the responsibility of the user to know the correct strings and usage of standard math functions and Adams variables/functions. To get the derived function string of a motion object for a result type, use UF_MOTION_get_object_derived_function. It is highly recommended that the syntax of a function definition be validated before creating the function object. See UF_MOTION_validate_function_syntax.
no automatic default naming, a new name
must be input for creation of function.