/*
 
uf_modl_dieeng.h
File description:
   Open API modeling routines to inquire about die engineering features.
*****************************************************************************/


#ifndef UF_MODL_DIEENG_H_INCLUDED
#define UF_MODL_DIEENG_H_INCLUDED


/***************************************************************************

 ***************************************************************************/


#include <uf_defs.h>
#include <libufun_exports.h>



/*
  Following is a structure definition for die tip feature inquiry data.
  It contains all the information needed to define the product orientation
  in the die.
*/


struct UF_MODL_die_tip_info_s
{
  tag_t product;                    /* Tag of product body being tipped */
  double origin[3];                 /* origin on product body that is
                                       mapped to center of operation box */

  double center[3];                 /* center of operation box */
  tag_t defining_tip_feature;       /* tag of feature that actually
                                       defined the product orientation,
                                       NULL_TAG if this feature defined
                                       the product orientation */

  double trans[3];                  /* translation from center of die */
  int num_trans_reasons;            /* number of strings in following array,
                                       will be 0 if no reasons supplied */
 
  char **trans_reasons;             /*  
                                       reasons supplied for translation,
                                       will be NULL if no reason,
                                       the memory for these strings should
                                       be freed by calling UF_free */

  int num_steps;                    /* number of steps in the product
                                       orientation definition, also the
                                       size of the following arrays */

  int *rot_axis;                    /*  
                                       for each step, the axis the
                                       rotation is performed about
                                       =0 -> X
                                       =1 -> Y
                                       =2 -> Z
                                       =3 -> -X
                                       =4 -> -Y
                                       =5 -> -Z,
                                       the memory for this array should
                                       be freed by calling UF_free */

  double *rot_angle;                /*  
                                       for each step, the angle of
                                       rotation in degrees, the memory
                                       for this array should be freed
                                       by calling UF_free */

  int *num_rot_reasons;             /*  
                                       number of reasons for each step,
                                       will be 0 if no reasons supplied
                                       for a step, the memory for this
                                       array should be freed by
                                       calling UF_free */

  char ***rot_reasons;              /*  
                                       for each step, the reasons supplied
                                       for the rotation, an entry will
                                       be NULL if no reasons, the memory
                                       for each string should be freed
                                       by calling UF_free, the string array
                                       should be freed by calling UF_free,
                                       and the complete array should also be
                                       freed by calling UF_free
                                       (e.g., UF_free(rot_reasons[0..n][0..n]);,
                                       UF_free(rot_reasons[0..n]);
                                       and UF_free(rot_reasons);) */

};
typedef struct UF_MODL_die_tip_info_s UF_MODL_die_tip_info_t,
*UF_MODL_die_tip_info_p_t;

/****************************************************************************
Outputs the product orientation information for the input die tip feature.

Return: error code

Environment: Internal  and  External

History: Original release was in V19.0
***************************************************************************/

extern UFUNEXPORT int UF_MODL_ask_die_tip(
   tag_t die_tip_feature, /* <I>
                             die tip feature to inquire
                          */

   UF_MODL_die_tip_info_p_t /* <OF>
                               die tip information
                            */

);



#undef EXPORTLIBRARY

#endif     /* UF_MODL_DIEENG_H_INCLUDED */