UF_MODL_vector_two_points_s
(view source)
Defined in: uf_modl_types.h
Also known as:
UF_MODL_vector_two_points_t
Overview
vector_type == UF_MODL_VECTOR_TWO_POINTS
Data Members
from_point [ 3 ]
double
Point coordinates from which the vector is to
start.
to_point [ 3 ]
double
Point coordinates at which the vector is to
end.
start.