This data is only used for the following mapping objects: Faces, Bodies, Sketches, Feature Curves, ... and Ouput objects of Smart Collectors.
output_objs_ss
struct UF_MODL_mapping_data_output_objs_ss_s
This data is only used for the following mapping objects: Output objects of Smart Sections (these objects are condemned, which are not displayed (i.e. invisible)).
Note that these output objects can't be used or destroyed for further applications.
data is only used for the following mapping objects:
Faces, Bodies, Sketches, Feature Curves, ... and
Ouput objects of Smart Collectors.