UF_MODL_stycorner_crv_opt_s (view source)
Defined in: uf_modl_types.h
Also known as:
- UF_MODL_stycorner_crv_opt
Overview
Structure to store the curve control option and corresponding
parameters for top curve, bottom curve, interior u-curve and
v-curve.
Data Members
shape_control
int
start_tagmag
double
end_tagmag
double
depth
double
skew
double
1: Tangent magnitude,
2: Template
If shape_control is 2 (template),
then there is no need to set
the rest of the data structure