UF_MODL_spherical_corner_s (view source)
Defined in: uf_modl_types.h
Also known as:
- UF_MODL_spherical_corner_t
- UF_MODL_spherical_corner_p_t
Overview
The data structure for the Spherical Corner feature. To create a feature,
a face collector for each wall must be provided. It can contain faces from
different bodies but the body being use to indicate the wall normal must be
specified through wall_x_ref_body and the reserve flag through is_wall_x_reversed.
When multiple solutions exist, a help point is required to determine the
nearest result.
Data Members
dist_tol
double
angle_tol
double
radius [ UF_MAX_EXP_BUFSIZE ]
char
wall_1
wall_2
wall_3
wall_1_ref_body
wall_2_ref_body
wall_3_ref_body
is_wall_1_reversed
is_wall_2_reversed
is_wall_3_reversed
help_point