Indication of whether this outline is defining the shape of the pocket/pad at the placement face of the pocket/pad, at the floor face o the pocket, or at the top face of the pad.
The parameter containing the angle value for the taper, if the taper_relative_to setting is UF_MODL_TAPER_BY_OUTLINE_FACE_NORMALS or UF_MODL_TAPER_BY_OUTLINE_FIXED_VECTOR then this should be an array of UF_MODL_parm_t where each is a law using the outline curve/edge as the spine
outline.