UF_MODL_shape_pattern_client_dialog_data_s (view source)
Defined in: uf_modl_types.h
Also known as:
- UF_MODL_shape_pattern_client_dialog_data_t
- UF_MODL_shape_pattern_client_dialog_data_p_t
Overview
The following data structure will be used to define client data for
the ShapePattern user interface dialog, that allows users to choose a thumbnail picture from a list
Environment
Internal & External
See Also
History
Originally released in NX503
Data Members
PartName
char *
HoleName
char *
iCountRecommendedShape
int
RecommendedShapeNames
char * *
RecommendedShapeThumbnailImageNames
char * *
RecommendedShapeLargeImageNames
char * *
iCountOtherShape
int
OtherShapeNames
char * *
OtherShapeThumbnailImageNames
char * *
OtherShapeLargeImageNames
char * *
NoImageBmpName
char *
CurrentHoleShapePatternName
char *
CurrentLargeImageName
char *
iSelectedHoleShapeIndex
int
bSelFromRecommendedGroup