UF_MODL_refit_face_target_data_s (view source)
 
Defined in: uf_modl_types.h
 
Also known as:
 
Overview
Following is a structure definition for refit face target data.

Parameters are to be specified as follows:
1.Number of target objects
2.Target objects
3.Fit direction
4.Maximum checking distance (any positive number)


Data Members

n_target_obj
int
Number of target objects

target_obj
tag_t *
Target objects

fit_direction_data
UF_MODL_refit_face_fit_direction_t
Fit direction

max_checking_data
double
Maximum checking distance