UF_MODL_mapping_data_output_objs_ss_s (view source)
Defined in: uf_modl_types.h
Overview
This data is only used for the following mapping objects:
Output objects of Smart Sections (these objects are condemned,
which are not displayed (i.e. invisible)).
Note that these output objects can't be used or destroyed
for further applications.
Data Members
old_output_objs_index
int *
new_output_objs_index
int *
of an old parent. To fill out this array, please
see the above comments.