UF_MODL_law_spine_s (view source)
Defined in: uf_modl_types.h
Also known as:
- UF_MODL_law_spine_t
- UF_MODL_law_spine_p_t
Overview
This structure defines a law, with a spine, in conjunction with the
UF_MODL_parm structure.
Note for all character string values in the structure, if the character
string is in expression format (e.g., p5=25, p5+p7), and the
expression does not exist, an expression is created and the law is
associated to that expression. If the expression does exist, then the
existing expression is edited, and the law is associated to that
expression. If the character string contains an expression name
(e.g., p5) and the expression exists, the law is associated to that
expression, if the expression does not exist an error occurs. If
the character string is a numeric value (e.g., 25), the law is not
associated to an expression.
Data Members
spine_profile
method_type
defined_by
spine of the law.