UF_MODL_law_no_spine_curve_s (view source)
Defined in: uf_modl_types.h
Also known as:
- UF_MODL_law_no_spine_curve_t
Overview
method_type == UF_MODL_LAW_CURVE. The law evaluates to the "Y" distance
between the given profile and the base curve, the profile should be in the
X-Y plane. If a base curve is not supplied, then the X axis is used as a base.
Data Members
law_profile
base
direction