UF_MODL_imprint_loop_data_s (view source)
 
Defined in: uf_modl_types.h
 
Also known as:
 
Overview
This structure contains the parametric information used to define an
imprint feature which will imprint edges on all the faces connected to
<imprint_face> which intersect with <imprint_datum_plane>. Hence it will
define a closed loop on the solid, even if the geometry of the solid is
later changed. It is an error if the face does not intersect
<imprint_datum_plane>.


Data Members

imprint_face
tag_t
The face defining the starting
point of the imprint

imprint_datum_plane
tag_t
The datum plane of intersection