UF_MODL_imprint_faces_data_s (view source)
 
Defined in: uf_modl_types.h
 
Also known as:
 
Overview
This structure contains the parametric information used to define an
imprint feature which will imprint an edge on every face in <imprint_faces>
where they intersect with <imprint_datum_plane>. The faces must all be on
the same body. It is an error if none of the faces intersect
<imprint_datum_plane>.


Data Members

n_imprint_faces
int
The number of faces

imprint_faces
tag_t *
Array of faces to be imprinted

imprint_datum_plane
tag_t
The datum plane of intersection