UF_MODL_gflange_sections_mode_data_s (view source)
 
Defined in: uf_modl_smd.h
 
Also known as:
 


Data Members

section_curves
UF_STRING_p_t
Each section must consist of curves
and/or edges that comprise an open G1
string. They must start tangent to
the target face. Each section must lie
in a plane that is normal to spine.
One end of the each section must touch
the bend edge.

extend_start
logical
TRUE = Maintain a constant section from
last defined section to the
spine start.
FALSE = To create generalized flange
till the last section near the
spine start

extend_end
logical
TRUE = Maintain a constant section
from last defined section to
the spine end.
FALSE = To create generalized flange
till the last section near
the spine end