UF_MODL_devchk_ee_info_s (view source)
 
Defined in: uf_modl_types.h
 
Also known as:
 


Data Members

dev_type
int
0 - no deviation
1 - step
2 - overlap
3 - gap

face_1_tag
tag_t
face tag on which edge_1_pnt lies

edge_1_pnt [ 3 ]
double
point on an edge of face_pairs[0] used for
deviation checking

norm_1 [ 3 ]
double
face normal at edge_1_pnt

face_2_tag
tag_t
face tag on which edge_2_pnt lies

edge_2_pnt [ 3 ]
double
point on an edge of face_pairs[1], where the
minimum deviation occured from edge_1_pnt

norm_2 [ 3 ]
double
face normal at edge_2_pnt

edge_dist
double
distance between edge_1_pnt and edge_2_pnt

norm_angle
double
Angle between the face normals