UF_MODL_curve_mesh_along_fixed_vector_data_s (view source)
Defined in: uf_modl_types.h
Also known as:
- UF_MODL_curve_mesh_along_fixed_vector_data_t
- UF_MODLcurve_mesh_along_fixed_vector_data__p_t
Overview
The following structure holds data that is specific to the
UF_MODL_curve_mesh_along_fixed_vector type of quilt surface.
This structure completely defines all creation parameters of this type
of surface.
Data Members
quilt_data
projection_vector [ 3 ]
double
primary_curves
cross_curves
elements of the quilt
feature.