UF_MODL_bracket_outline_data_s (view source)
 
Defined in: uf_modl_smd.h
 
Also known as:
 


Data Members

reference_geometry_type
int
0 = Clearance Points, 1 = Edge,
2 = Length. The user can specify
either clearance points to
define the outline, select
an edge or specify a
length (pad or flange)

num_clr_pts
int
Number of clearance points on the
reference/base face. This number
is used only when
reference_geometry_type = 0 ,
i.e when clearance points are
specified . The minimum number of
points can be one and maximum of
two points

data
union UF_MODL_bracket_outline_data_union