UF_MODL_b_surface_along_fixed_vector_data_s (view source)
Defined in: uf_modl_types.h
Also known as:
- UF_MODL_b_surface_along_fixed_vector_data_t
- UF_MODL_b_surface_along_fixed_vector_data_p_t
Overview
The following structure holds data that is specific to the
UF_MODL_b_surface_along_fixed_vector type of quilt surface. This
structure completely defines all creation parameters of this type of
surface.
Data Members
quilt_data
projection_vector [ 3 ]
double
driver_surface
elements of the quilt
feature.