UF_MB_action_type_e (view source)
Defined in: uf_mb.h
Also known as:
- UF_MB_action_type_t
- UF_MB_action_type_p_t
Overview
Each member of the UF_MB_action_type_t enumerated type represents
one of the action types that can be specified for an action declared
in a MenuScript menu file. This enumerated type is reserved for
future use in the Open API; currently it is only used internally
within MenuScript.
Data Members
UF_MB_FUNCTION_ACTION
UF_MB_PROGRAM_ACTION
UF_MB_GRIP_ACTION
UF_MB_JOURNAL_ACTION = UF_MB_GRIP_ACTION
UF_MB_IMMEDIATE_ACTION
UF_MB_USER_TOOL_ACTION
UF_MB_STYLER_DIALOG_ACTION
UF_MB_STYLER_TOP_DIALOG_ACTION
UF_MB_LEGACY_ACTION
UF_MB_cb_status_e (view source)
Defined in: uf_mb.h
Also known as:
- UF_MB_cb_status_t
- UF_MB_cb_status_p_t
Overview
Each member of the UF_MB_cb_status_t enumerated type represents one
of the possible return values from a callback function that has been
registered via UF_MB_add_actions.
To support possible future semantic differences between return codes, the
five values shown below have been defined. The comments next to each
member identify its nominal meaning. However, there are currently only
two sets of semantics associated with these five values:
UF_MB_CB_CONTINUE - this value will cause execution of any additional
actions for a menu item to be executed.
Any of the other four values will inhibit execution of the remaining
actions.
Data Members
UF_MB_CB_CONTINUE
UF_MB_CB_CANCEL
UF_MB_CB_OVERRIDE_STANDARD
UF_MB_CB_WARNING
UF_MB_CB_ERROR
UF_MB_state_e (view source)
Defined in: uf_mb.h
Also known as:
- UF_MB_state_t
- UF_MB_state_p_t
Overview
The elements of the UF_MB_state_t enumerated type correspond to
ask or set routine argument for a button's sensitivity or a toggle
button's current state.
Data Members
UF_MB_ON
UF_MB_OFF
UF_MB_add_actions