UF_MB_styler_actions_s (view source)
Defined in: uf_mb.h
Also known as:
- UF_MB_styler_actions_t
- UF_MB_styler_actions_p_t
Overview
The following structure is used to associate the callbacks of a UIStyler
dialog to a menubar action. This structure is used with the function
UF_MB_add_styler_actions. You must have associated your UIStyler dlg file to
a push button using MenuScript in order to use UF_MB_add_styler_actions.
Please note that the information for this structure is automatically provided
to you in your template source file.
Data Members
styler_file
char *
client_data
void *
callback_list
is_top_dialog
int
associate your callbacks with.