UF_MB_application_data_s (view source)
Defined in: uf_mb.h
Also known as:
- UF_MB_application_t
- UF_MB_application_p_t
Overview
The UF_MB_application_t structure is used to register a custom
application with NX and specify its characteristics.
Data Members
id
int
name
char *
init_proc
exit_proc
enter_proc
drawings_supported
design_in_context_supported
supports_undo
to the custom application by
NX. There are currently no
MenuScript API routines that use this
value, but there may be in
the future. This is returned by the
UF_MB routines.