/*
uf_lib.h
* File description:
*
* This file contains documentation for the UF_LIB module. This module
* allows the Open API programmer to interface with the Libraries that NX
* uses for retrieving objects such as Machine Tools, Cutters, Tool
* Material and Feeds and Speeds. The programmer can perform functions
* such as retrieving objects into NX and asking for the values of
* attributes of objects in a Library.
*
* The query syntax:
*
* An application can create a query that contains the constraints which
* should be used in selecting objects in the Library. The query must be
* specified using the query language. The language of a query is very
* simple. It is a collection of criteria which are connected to each other
* with certain logical operators. A criterion has the form:
*
* [Attribute Name] [Relational Operator] [Expression]
*
* where a(n)
*
* [Attribute Name] is an NX name of one of the database attributes of the
* objects being queried,
*
*
* [Relational Operator] is one of <, <=, ==, !=, >, >=, &=, &!,
*
* [Expression] is an expression made up of (primarily) NX Expression
* SubSystem (ESS) expressions and NX Names.
*
* If the operator is &= or &! then [Expression] is an egrep style regular
* expression (see man pages on egrep or TCL regular expressions). We
* describe these expressions in more detail below.
*
* The Relational Operators &= and &! mean String Equal and String Not
* Equal, resp.
*
* The logical operators allowed are && and || with && having
* precedence over ||.
*
* An NX name is a non database-specific name for an attribute of an object
* that is stored in a library. (These names are defined in the Definition
* File of the DBC object used for the query.) For example, a query might
* use Tool_Diameter to specify the diameter of the tool, whereas, Genius
* may use a UNCT of -1001 to denote the tool diameter. In this case
* Tool_Diameter is the NX Name.
*
* The query language places very few restrictions on the form of an
* [Expression].
* The restrictions are:
*
* 1) each occurrence of an NX ESS expression must be surrounded by
* delimiters and,
*
* 2) each occurrence of an NX name must be surrounded by delimiters.
* (The delimiters are also defined in the Definition File of the DBC
* object used for the query.)
*
* 3) the entire [Expression] must be a valid TCL expression.
*
* In the following examples of QRY queries, we use DB( and ) as the NX Name
* start and end delimiters, resp., and ESS( and ) as the ESS start and end
* delimiters, resp. These are user-defined via the DBC Definition File
*
* Here are 2 examples of QRY queries:
*
* [DB(Tool_Diameter)] >= [0.25] && [DB(Tool_Diameter)] <= [0.50]
*
* [DB(Tool_Diameter)] < [2 * ESS(Corner_Radius)] &&
* [DB(Num_Of_Flutes)] == [3 * ESS(Height)] && [DB(Material)] &=
* ["^STEEL[123]$"] && [DB(Catalog)] &! ["^.*VENDOR_A.*$"]
*
******************************************************************************/
#ifndef UF_LIB_H_INCLUDED
#define UF_LIB_H_INCLUDED
/***************************** Include Files **********************************/
#include <uf_defs.h>
#include <uf_cam.h>
#include <libufun_exports.h>
/***************************** Public Typedefs ********************************/
/* This data type is the result of a query. The elements of this type may be
* queried with UF_LIB_ask_record_in_rset() and UF_LIB_ask_rset_map().
*/
typedef void *UF_RSET_t;
/************************* Public Function Definitions ************************/
/*****************************************************************************
* This function will execute a query in a library and return a count of the
* number of objects in the library that satisfy the query. See the above
* File Description for a discussion of the query syntax. The Class Query in
* the Definition File is &&ed to the query specified here as a parameter.
*
*
* Environment : Internal and External
* See Also:
* History : Released in V16.0
****************************************************************************/
extern UFUNEXPORT int UF_LIB_execute_query_for_count
(
UF_CAM_db_object_t db, /* <I> - the library object in which to
execute the query */
const char *cls_name, /* <I> - the class name */
const char *query, /* <I> - the query */
int *count /* <O> - the number of objects in the library that
* satisfy the query.
*/
);
/*****************************************************************************
* This function returns the number of records that the specified UF_RSET_t
* contains.
*
* Environment : Internal and External
* See Also:
* History : Released in V17.0
****************************************************************************/
extern UFUNEXPORT int UF_LIB_ask_rset_count
(
UF_RSET_t rset, /* <I> - the UF_RSET_t whose record count is desired */
int *count /* <O> - the number of records in the UF_RSET_t */
);
/*****************************************************************************
* This function will execute a query in a library and return a record set
* containing the objects in the library that satisfy the query.
* See the above File Description for a discussion of the query syntax. The
* Class Query in the Definition File is &&ed to the query specified here as
* a parameter. The contents of the RSET returned is determined by the
* RSET definition for the specified class name. This definition is found in the
* Definition File.
*
* Environment : Internal and External
* See Also:
* History : Released in V16.0
****************************************************************************/
extern UFUNEXPORT int UF_LIB_execute_query
(
UF_CAM_db_object_t db, /* <I> - the library object in which to
execute the query. */
const char *cls_name, /* <I> - the class name */
const char *query, /* <I> - the query */
int *count, /* <O> - the number of objects satisfying the query */
UF_RSET_t *rset /* <O> - the record of objects that satisfy
the query */
);
/*****************************************************************************
* This function provides a description (or map) of the contents of a record
* set. It provides a list of the attributes that each record in the record
* set has as well as the type of each of those attributes. One can think of
* a record set as a table. The rows of the table are the individual records
* in the record set. The columns headings are the attributes that are found
* in the record set.
*
* E.g.:
*
* libref Tool Name Diameter Material
* --------------------------------------
* ref1 Drill 3.5 Steel
* ref2 Mill 1.3 Alloy
*
* In this record set the attributes are:
* libref, Tool Name, Diameter and Material and
* the types are: s, s, d, s.
*
* The type characters are: s == string
* i == integer
* d == double
*
*
****************************************************************************/
/*****************************************************************************
* This function provides a description (or map) of the contents of a record
* set. It provides a list of the attributes that each record in the record
* set has as well as the type of each of those attributes. One can think of
* a record set as a table. The rows of the table are the individual records
* in the record set. The columns headings are the attributes that are found
* in the record set.
* NOTE: Use UF_LIB_free_rset_map to free returned memory
* See the description
* Environment : Internal and External
* See Also: UF_LIB_free_rset_map
* History : Released in V16.0
****************************************************************************/
extern UFUNEXPORT int UF_LIB_ask_rset_map
(
UF_RSET_t rset, /* <I> - the record set of interest. This was
* returned by execute_query.
*/
int *count, /* <O> - the number of attributes in the record
* set.
*/
const char ***attr_names, /* <OF> count - the name of the attributes in the
record set.
*/
const char **attr_types /* <OF> count - the types of the attributes. The ith
* attr_types is the type of the ith
* attr_names.
*/
);
/*****************************************************************************
* This function frees the memory returned from UF_LIB_ask_rset_map
*
* Environment : Internal and External
* See Also: UF_LIB_ask_rset_map
* History : Released in V16.0
****************************************************************************/
extern UFUNEXPORT int UF_LIB_free_rset_map
(
int count, /* <I> - the number of attributes in the record set. */
const char **attr_names, /* <I> - the name of the attributes in the record
* set. */
const char *attr_types /* <I> - the types of the attributes. The ith
* attr_types is the type of the ith
* attr_names. */
);
/*****************************************************************************
* This function provides a record from a record set. The record is returned
* as an array of strings. Each element of the array is the value of an
* attribute of the specified record. The ith element of the array is the
* value of the ith attribute returned from ask_rset_map. Note that all values
* are returned as strings. If the value has type double or int the caller
* will need to convert as required by the application.
*
* The caller should use UF_free_string_array to free these returned arrays.
*
* Environment : Internal and External
* See Also:
* History : Released in V16.0
****************************************************************************/
extern UFUNEXPORT int UF_LIB_ask_record_in_rset
(
UF_RSET_t rset, /* <I> - the desired record set */
int record_num, /* <I> - the desired record number (0 based) */
int *count, /* <O> - the number of values of attributes */
const char ***values /* <OF> - the values of the attributes. The
caller should call UF_free_string_array
to free this array. */
);
/*****************************************************************************
* This function sorts the contents of a record set. The sort key is of the
* form:
*
* db_alias1/{a|d},db_alias2/{a|d},...,db_aliasN/{a|d}
*
* where a = ascending, d = descending. For example, if Diameter and Cost are
* both DB Aliases that are found in the record set one could sort the set
* primarily by Diameter in ascending order and then, within Diameter, sort by
* Cost in decreasing order with a sort key of:
*
* Diameter/a,Cost/d
*
* Here Diameter is the primary key. Records of the set that have the same
* Diameter are then sorted by Cost. The original record set is not changed.
*
* Environment : Internal and External
* See Also:
* History : Released in V17.0
****************************************************************************/
extern UFUNEXPORT int UF_LIB_sort_rset
(
UF_RSET_t rset, /* <I> - the record set to sort */
const char *sort_key, /* <I> - the sort key to sort by */
UF_RSET_t *sorted_rset /* <O> - the sorted record set */
);
/*****************************************************************************
* This function merges the contents of two record sets. The merged record set
* contains the records of 'rset1' followed by the records of 'rset2'. The
* records appear in the same order they did in their original record sets.
* 'rset1' and 'rset2' are unchanged.
*
* Environment : Internal and External
* See Also:
* History : Released in V17.0
****************************************************************************/
extern UFUNEXPORT int UF_LIB_merge_rsets
(
UF_RSET_t rset1, /* <I> - the record set to merge */
UF_RSET_t rset2, /* <I> - the other record to merge */
UF_RSET_t *merged_rset /* <O> - the merged record set */
);
/*****************************************************************************
* This function deletes the specified UF_RSET_t.
*
* Environment : Internal and External
* See Also:
* History : Released in V17.0
****************************************************************************/
extern UFUNEXPORT int UF_LIB_delete_rset
(
UF_RSET_t rset /* <I> - the record set to delete */
);
/*****************************************************************************
* This function provides the library reference (or libref) of the specified
* NX object. The libref is an attribute which is returned for every record
* in every record set. It is also the attribute which is used to retrieve
* an object from a library. An NX object will only have a libref if it was
* created by being retrieved from a library.
*
* Environment : Internal and External
* See Also:
* History : Released in V16.0
****************************************************************************/
extern UFUNEXPORT int UF_LIB_ask_libref
(
tag_t ug_object, /* <I> - the desired NX object */
const char **libref /* <OF> - the libref of the specified object */
);
/*****************************************************************************
* This function provides a list of attribute values of an NX object that
* was previously retrieved from a library. The library is referenced by the
* specified UF_CAM_db_object_t. The values are the current values (in the
* library) of the specified attributes of the NX object.
*
* The caller should use UF_free_string_array to free these returned arrays.
*
* Environment : Internal and External
* See Also:
* History : Released in V16.0
****************************************************************************/
extern UFUNEXPORT int UF_LIB_ask_lib_attribute_values
(
UF_CAM_db_object_t db, /* <I> - the db object to query in */
tag_t ug_object, /* <I> - the NX object to query about */
int count, /* <I> - the number of attribute to ask their
* values of */
const char **db_alias, /* <I> - the list of attribute db aliases to
* ask the values of */
char ***values /* <OF> - the requested values. This is
an array of strings that must be freed
by calling UF_free_string_array. */
);
#undef EXPORTLIBRARY
#endif /* UF_LIB_H_INCLUDED */