UF_GDT_surface_parms_s
(view source)
Defined in: uf_gdt.h
Also known as:
UF_GDT_surface_parms_t
UF_GDT_surface_parms_p_t
Overview
Defines the surfaces of a feature. These are used by the ask, create, and
set routines for tolerance feature. They are also used to define the
origin surfaces for directed dimensions.
Functions affected by the modification of this structure are:
UF_GDT_ask_directed_dimension
UF_GDT_ask_feature_parms
UF_GDT_create_datum_identifier
UF_GDT_create_fcf
UF_GDT_create_instance
UF_GDT_create_size_tolerance
UF_GDT_set_directed_dimension
Data Members
num_faces
int
Number of faces that define
the current surface
faces
tag_p_t
Set of face tags
the current surface