UF_GDT_modl_data_s (view source)
Defined in: uf_gdt.h
Also known as:
- UF_GDT_modl_data_t
- UF_GDT_modl_data_p_t
Overview
The following data structure contains modeling feature data. Currently,
tolerance feature can reference following NX modeling features -
1. Simple Hole
2. Counterbore Hole
3. Countersink Hole
4. Extrusion/Revolution
5. Boss
6. Edge Blend
7. Rectangular Pad
8. Rectangular Slot
9. Ball End Slot
10. U Slot
11. T Slot
12. Cylindrical Pocket
13. Rectangular Pocket
14. Symbolic Thread
This data can be used in create/ask/set routines for modeling based
tolerance features.
Data Members
num_modl_features
int
modl_feature_list
modl_param
face_map