UF_GDT_description_s (view source)
Defined in: uf_gdt.h
Also known as:
- UF_GDT_description_t
- UF_GDT_description_p_t
Overview
Defines the attributes required to describe a tolerance feature
Alternatively the name and description of the tolerance feature may be
manipulated directly using character strings and the UF_OBJ_read/write
routines
Data Members
name
char *
description
char *
NOTE :
. The name supplied may not be NULL.
. The name supplied must be unique within the
context of the tolerancing module.
. The name must be less than 31 characters in length.