UF_FAM_family_data_s
(view source)
Defined in: uf_fam_types.h
Also known as:
UF_FAM_family_data_t
UF_FAM_family_data_p_t
Data Members
subtype
int
A flag indicating which type of family
this is. Currently this can only be set to
UF_fam_part_subtype
attribute_count
int
The number of attributes of the
family.
member_count
int
The number of members in the family.
attributes
tag_t *
An array of family attribute tags which
describe the parameters of the family.
name
char *
The name for the family.
this is. Currently this can only be set to
UF_fam_part_subtype