UF_EVAL_arc_s (view source)
 
Defined in: uf_eval.h
 
Also known as:
 


Data Members

is_periodic
logical
Is the curve periodic or not?

limits [ 2 ]
double
Curve limits (in radians): [0] = min; [1] = max

radius
double
Radius

center [ 3 ]
double
Center (ABS coordinates)

x_axis [ 3 ]
double
Unit direction vector of the x axis (ABS)

y_axis [ 3 ]
double
Unit direction vector of the y axis (ABS)