UF_DRPOS_feed_unit_e (view source)
Defined in: uf_drpos.h
Also known as:
Overview
UF_DRPOS_feed_unit_t enumerates the available set of units in
which the feed rate may be expressed
Data Members
UF_DRPOS_FEED_UNIT_NONE = 0
UF_DRPOS_FEED_UNIT_PER_MIN = 1
UF_DRPOS_FEED_UNIT_PER_REV = 2
UF_DRPOS_feed_use_e (view source)
Defined in: uf_drpos.h
Also known as:
Overview
UF_DRPOS_feed_use_t enumerates the available options for how to
obtain the feed rate for a UF_DRPOS object
Data Members
UF_DRPOS_FEED_USE_DEFAULT = 0
UF_DRPOS_FEED_USE_CUSTOM = 1
UF_DRPOS_type_e (view source)
Defined in: uf_drpos.h
Also known as:
Overview
UF_DRPOS_type_t enumerates the different types of UF_DRPOS objects
Data Members
UF_DRPOS_TYPE_NONE = 0
UF_DRPOS_TYPE_CUT = 1
UF_DRPOS_TYPE_FIRST_CUT = 2
UF_DRPOS_TYPE_STEPOVER = 10
UF_DRPOS_TYPE_LOCAL_LIFT = 50
UF_DRPOS_TYPE_FINAL_LIFT = 51
UF_DRPOS_zig_zag_dir_e (view source)
Defined in: uf_drpos.h
Also known as:
Overview
UF_DRPOS_zig_zag_dir_t enumerates the two directions of cut
when doing zig/zag type cut patterns
Data Members
UF_DRPOS_ZIG_ZAG_DIR_ZIG = 0
UF_DRPOS_ZIG_ZAG_DIR_ZAG = 1