UF_DRF_uds_size_s (view source)
 
Defined in: uf_drf_types.h
 
Also known as:
 
Overview
Structure defining the length / height or scale / aspect ratio parameters
of embedded or standalone symbols.


Data Members

uds_size_type
UF_DRF_uds_size_type_t
If the uds type is set to UF_DRF_LENGTH_HEIGHT, then the following
parameters are interpreted as ?length and height?. If the uds
type is set to UF_DRF_SCALE_ASPECT_RATIO, then the following
parameters are interpreted as ?scale and aspect ratio?.

length_or_scale
double


height_or_aspect_ratio
double