UF_DRF_symbol_instance_s (view source)
 
Defined in: uf_drf_types.h
 
Also known as:
 
Overview
This is a structure to hold embedded user defined symbol
History - This structure was originally released in V15.0.


Data Members

master
tag_t
master symbol

is_gap
logical
TRUE if a gap, else FALSE

origin [ 3 ]
double
symbol origin in csys of annotation

parameter_on_element
double
normalized parameter on line or arc

symbol_length
double
length of symbol

symbol_height
double
height of symbol

creation_mask
int
symbol creation mask

record_number
int
record number in owning component

segment_number
int
segment number of owning component
segment

is_mirrored
logical
TRUE if reflected about its X axis

is_reflected
logical
TRUE if reflected about line between
anchor and connection pt