UF_DRF_lettering_preferences_s (view source)
 
Defined in: uf_drf_types.h
 
Also known as:
 
Overview
UF_DRF_lettering_preferences_t specifies the lettering preferences for
dimension text, appended text, tolerance text, and general text.


Data Members

align_position
UF_DRF_align_position_t
one of nine site locations in
the text rectangle used to
place the text

horiz_text_just
UF_DRF_text_just_t
horizontal text
justification

gdt_frame_height_factor
double
GD&T frame height
factor

angle
double
angle for general text

dimension_text
UF_DRF_lettering_t
lettering preferences for
dimension text

appended_text
UF_DRF_lettering_t
lettering preferences for
appended text

tolerance_text
UF_DRF_lettering_t
lettering preferences for
tolerance text

general_text
UF_DRF_lettering_t
lettering preferences for
drafting aid text

dim_dim_line_space_factor
double
this controls spacing between bottom most piece of text on the dimension
and the dimension line when text orientation is
UF_DRF_DIMENSION_TEXT_OVER_DIMENSION_LINE. This factor is applied to the
dimension text character size to determine the spacing

dim_app_text_space_factor
double
controls spacing between before appended text and next piece of
dimension text to its right, and spacing between the after appended
text and next piece of dimension text to its left. This factor is
applied to the appended text character size to determine the spacing

dim_tol_text_space_factor
double
controls spacing between dimension main text and after tolerance text.
this factor is applied to the tolerance text character size to determine
the spacing