UF_DRF_draft_aid_line_s (view source)
Defined in: uf_drf_types.h
Also known as:
- UF_DRF_draft_aid_line_t
- UF_DRF_draft_aid_line_p_t
Overview
This is a structure to hold drafting aid line information
History - V15.0 change: The following fields were added: sequence_number,
num_symbols, and symbol_data.
V17.0 segment_pnts is now dynamically allocated.
the minimum size will be its previous fixed size
which was MAX_LINE_NCHARS 6.
Data Members
sequence_number
int
num_symbols
int
symbol_data
num_segments
int
segment_pnts
double *
numbers per line