UF_DRF_diameter_radius_preferences_s (view source)
 
Defined in: uf_drf_types.h
 
Also known as:
 
Overview
UF_DRF_diameter_radius_preferences_t specifies annotation preferences
that only apply to radial type dimensions


Data Members

diameter_symbol_type
UF_DRF_diameter_symbol_t
standard diameter symbol or
user-defined

diameter_symbol [ UF_DRF_DIAMETER_RADIUS_SYMBOL_MAX_BUFSIZE ]
char
text for user-defined diameter symbol

radius_symbol_type
UF_DRF_radius_symbol_t
standard radius symbol or
user-defined

radius_symbol [ UF_DRF_DIAMETER_RADIUS_SYMBOL_MAX_BUFSIZE ]
char
text for user-defined radius symbol

diameter_radius_placement
UF_DRF_diameter_radius_placement_t
placement of diameter/radius symbol
relative to dimension text

text_above_leader
UF_DRF_text_above_leader_t
if option is set to anything other than
UF_DRF_NO_TEXT_ABOVE_LEADER, then
dimension text will be displayed above
the leader stub with the stub extended
to the maximum length of the dimension
text. used with dimension text
orientations of
UF_DRF_TEXT_DIMENSION_HORIZONTAL and
UF_DRF_TEXT_DIMENSION_BY_ANGLE.
for UF_DRF_NO_TEXT_ABOVE_LEADER, the
dimension text displays next to the
leader stub

symbol_to_dimension_text_distance
double
distance between radius/
diameter symbol and dimension
text in character spaces

folded_radius_angle
double
angle of the fold for folded radius
dimensions