UF_DRF_arc_info_s (view source)
 
Defined in: uf_drf_types.h
 
Also known as:
 
Overview
This is a structure to hold arc data
History - V15.0 change: The following fields were added: arc_type,
sequence_number, num_symbols, and symbol_data.


Data Members

arc_type
int
arc type

sequence_number
int
arc sequence number

arc_center [ 3 ]
double
x, y coordinate

radius
double
arc radius

start_angle
double
arc start angle

end_angle
double
arc end angle

num_symbols
int
number of User Defined
Symbols

symbol_data
UF_DRF_symbol_instance_t *
User Defined Symbol
data

num_assoc_objs
int
number of associated
objects

assoc_objs
UF_DRF_assoc_info_t *
leader assoc object tag
type, and modifier