UF_DIE_wrap_binder_union
(view source)
Defined in: uf_dieeng.h
Data Members
points
struct UF_DIE_wrap_binder_defining_points_s
use the following structure when input_type == UF_DIEENG_POINTS
string
struct UF_DIE_wrap_binder_defining_string_s
use the following structure when input_type == UF_DIEENG_BOUNDARY
sheet
struct UF_DIE_wrap_binder_sheet_body_s
use the following structure when input_type == UF_DIEENG_SHEET