A string of objects defining the binder outline. This structure can contain a combination of curves, edges, curve features, a single face, and sketches. If features are included then the curves produced by that feature are input. If sketches are included then the curves in the sketch are input. If a single face is included then the edges of the face are input.
outline. This structure can contain a
combination of curves, edges, curve features,
a single face, and sketches. If features are
included then the curves produced by that
feature are input. If sketches are included
then the curves in the sketch are input. If a
single face is included then the edges of the
face are input.