UF_CURVE_ocf_values_s (view source)
Defined in: uf_curve.h
Also known as:
- UF_CURVE_ocf_values_t
- UF_CURVE_ocf_values_p_t
Overview
Structure that holds the offset value for a given string in an associated
offset curve in face feature. The offset value is stored as a string.
Data Members
string [ MAX_FSPEC_BUFSIZE ]
char
hold an offset value in
form of a string (e.g "2.0")
to offset the string on the
input set of faces.