UF_CURVE_constraint_s (view source)
 
Defined in: uf_curve.h
 
Also known as:
 
Overview
The following structure is the structure used define the constraint
with which the associative curve must be created.


Data Members

constraint_type
UF_CURVE_constraint_type_t
The type of constraint

end_type
UF_CURVE_end_type_t
The end to which this constraint
must be applied.

object_tag
tag_t
Object with which the constraint
is to be applied.

value
double
If constraint needs a value then
use this field, ex. UF_CURVE_angle
UF_CURVE_radius type constraints.

help_data
UF_CURVE_help_data_t
help data when constraint is tangent / normal