UF_CLONE_log_file_failure_s (view source)
Defined in: uf_clone.h
Also known as:
- UF_CLONE_log_file_failure_t
- UF_CLONE_log_file_failure_p_t
Overview
structure used to report extra details of an error detected when
reading a log file, supplementary to the information given by applying
UF_get_fail_message to the return code of the UF_CLONE_load_logfile
call
Data Members
line_number
int
input_part_name
char *
invalid_token
char *
line number in the log file on which the error
was detected