UF_CLONE_copy_nm_opt_s (view source)
Defined in: uf_clone.h
Also known as:
- UF_CLONE_copy_nm_opt_t
- UF_CLONE_copy_nm_opt_p_t
Overview
UF_CLONE_copy_nm_opt_t: Element of a linked list setting the
flag for a specific non-master type to indicate whether or not it
should be copied during a clone, import or export operation, the
list is terminated by setting the next field of this structure to
NULL. This structure can be either an input argument to a _set_
function or an output argument of an _ask_ function.
Data Members
nonmaster_type
char *
copy
next
struct UF_CLONE_copy_nm_opt_s *
returned a string containing the name of a
nonmaster type defined in the database, such as
"specification"