UF_CGM_ask_default_custom_colors (view source)
Defined in: uf_cgm.h
Overview
Returns the default CGM export custom colors.
Environment
Internal and External
See Also
History
Originally released in NX3.0.
Required License(s)
gateway
int UF_CGM_ask_default_custom_colors
(
UF_CGM_custom_colors_p_t custom_colors
)
UF_CGM_ask_default_custom_widths (view source)
Defined in: uf_cgm.h
Overview
Returns the default CGM export custom widths.
Environment
Internal and External
See Also
History
Originally released in NX3.0.
Required License(s)
gateway
int UF_CGM_ask_default_custom_widths
(
UF_CGM_custom_widths_p_t custom_widths
)
UF_CGM_ask_default_export_options (view source)
Defined in: uf_cgm.h
Overview
Returns the default CGM export option settings.
Environment
Internal and External
See Also
History
Originally released in NX3.0.
Required License(s)
gateway
int UF_CGM_ask_default_export_options
(
UF_CGM_export_options_p_t export_options
)
UF_CGM_ask_session_custom_colors (view source)
Defined in: uf_cgm.h
Overview
Returns the current CGM export custom colors for the session.
Environment
Internal and External
See Also
History
Originally released in NX3.0.
Required License(s)
gateway
int UF_CGM_ask_session_custom_colors
(
UF_CGM_custom_colors_p_t custom_colors
)
UF_CGM_ask_session_custom_widths (view source)
Defined in: uf_cgm.h
Overview
Returns the current CGM export custom widths for the session.
Environment
Internal and External
See Also
History
Originally released in NX3.0.
Required License(s)
gateway
int UF_CGM_ask_session_custom_widths
(
UF_CGM_custom_widths_p_t custom_widths
)
UF_CGM_ask_session_export_options (view source)
Defined in: uf_cgm.h
Overview
Returns the current CGM export option settings for the session.
Environment
Internal and External
See Also
History
Originally released in NX3.0.
Required License(s)
gateway
int UF_CGM_ask_session_export_options
(
UF_CGM_export_options_p_t export_options
)
UF_CGM_export_cgm (view source)
Defined in: uf_cgm.h
Overview
Exports a CGM file with the specified name. Suffix .cgm is appended to
the name if not present. If a CGM file of the same name already exists,
it is overwritten. The drawing sheet provided must be in the displayed
part.
Environment
Internal and External
See Also
History
Originally released in NX3.0.
Required License(s)
gateway
int UF_CGM_export_cgm
(
tag_t drawing_sheet,
UF_CGM_export_options_p_t export_options,
const char * file_name
)
tag_t | drawing_sheet | Input | The tag of the drawing sheet to export. If set to NULL_TAG, the current display image is exported instead. |
UF_CGM_export_options_p_t | export_options | Input | Specifies export options. If NULL, current session export options are used instead. If non-NULL, call UF_CGM_ask_default_export_options or UF_CGM_ask_session_export_options to initialize the structure before setting structure fields. Current session export options are not modified by structure values. |
const char * | file_name | Input | The CGM filename |
UF_CGM_import_cgm (view source)
Defined in: uf_cgm.h
Overview
Imports the CGM file with the specified name.
Environment
Internal and External
See Also
History
Originally released in NX3.0.
Required License(s)
gateway
int UF_CGM_import_cgm
(
char * file_name,
UF_CGM_import_options_p_t import_options
)
char * | file_name | Input | The CGM filename |
UF_CGM_import_options_p_t | import_options | Input | Specifies import options. If NULL, default import options are used instead. If non-NULL, call UF_CGM_init_import_options to initialize the structure before setting structure fields. |
UF_CGM_init_import_options (view source)
Defined in: uf_cgm.h
Overview
Initializes the fields of a UF_CGM_import_options_t structure to default
values. Call this function before setting structure fields in preparation
to call UF_CGM_import_cgm.
Environment
Internal and External
See Also
History
Originally released in NX3.0.
Required License(s)
gateway
int UF_CGM_init_import_options
(
UF_CGM_import_options_p_t import_options
)
UF_CGM_register_callbacks (view source)
Defined in: uf_cgm.h
Overview
Registers functions to be called when exporting a CGM starts or stops.
Environment
Internal and External
History
Originally released in NX6.0.4
Required License(s)
gateway
int UF_CGM_register_callbacks
(
UF_CGM_pre_export_f_t pre_export,
UF_CGM_post_export_f_t post_export,
UF_CGM_export_error_f_t export_error
)
UF_CGM_set_session_custom_colors (view source)
Defined in: uf_cgm.h
Overview
Modifies the current CGM export custom colors for the session. Call
one of the following functions to initialize the UF_CGM_custom_colors_t
structure before setting structure fields.
UF_CGM_ask_default_custom_colors
UF_CGM_ask_session_custom_colors
UF_PLOT_ask_drawing_sheet_colors
UF_PLOT_read_custom_colors_from_cdf
Environment
Internal and External
See Also
History
Originally released in NX3.0.
Required License(s)
gateway
int UF_CGM_set_session_custom_colors
(
UF_CGM_custom_colors_p_t custom_colors
)
UF_CGM_set_session_custom_widths (view source)
Defined in: uf_cgm.h
Overview
Modifies the current CGM export custom widths for the session. Call
one of the following functions to initialize the UF_CGM_custom_widths_t
structure before setting structure fields.
UF_CGM_ask_default_custom_widths
UF_CGM_ask_session_custom_widths
UF_PLOT_ask_drawing_sheet_widths
UF_PLOT_read_custom_widths_from_wdf
Environment
Internal and External
See Also
History
Originally released in NX3.0.
Required License(s)
gateway
int UF_CGM_set_session_custom_widths
(
UF_CGM_custom_widths_p_t custom_widths
)
UF_CGM_set_session_export_options (view source)
Defined in: uf_cgm.h
Overview
Modifies the current CGM export option settings for the session. Call
UF_CGM_ask_default_export_options or UF_CGM_ask_session_export_options
to initialize the UF_CGM_export_options_t structure before setting
structure fields.
Environment
Internal and External
See Also
History
Originally released in NX3.0.
Required License(s)
gateway
int UF_CGM_set_session_export_options
(
UF_CGM_export_options_p_t export_options
)
UF_CGM_unregister_callbacks (view source)
Defined in: uf_cgm.h
Overview
Unregisters functions to be called when exporting a CGM starts or stops.
Environment
Internal and External
History
Originally released in NX6.0.4
Required License(s)
gateway
int UF_CGM_unregister_callbacks
(
UF_CGM_pre_export_f_t pre_export,
UF_CGM_post_export_f_t post_export,
UF_CGM_export_error_f_t export_error
)
UF_CGM_pre_export_f_t | pre_export | Input | The function previously registered to be called when a CGM export is started. |
UF_CGM_post_export_f_t | post_export | Input | The function previously registered to be called when a CGM export is finished. |
UF_CGM_export_error_f_t | export_error | Input | The function previously registered to be called when a CGM export gets an error. |