UF_CGM_dimensions_s (view source)
Defined in: uf_cgm_types.h
Also known as:
- UF_CGM_dimensions_t
- UF_CGM_dimensions_p_t
Overview
Structure UF_CGM_dimensions_t specifies the dimensions of CGM
geometry recorded in the CGM file. The dimensions field of the
UF_CGM_size_t structure is a structure of type UF_CGM_dimensions_t.
The dimensions field of the UF_CGM_dimensions_t structure specifies
the width and height of CGM geometry, expressed in the units indicated
by the units field.
Data Members
units
dimensions [ 2 ]
double