UF_OPRBND_app_data_s (view source)
Defined in: uf_oprbnd.h
Also known as:
- UF_OPRBND_app_data_t
- UF_OPRBND_app_data_p_t
Overview
The application data for a inherited boundary and the members:
The following information shows the types of application data
allowed by the objects and the boundary types.
An error code is returned by the functions if a wrong type
of application data is set.
Facing Operation Boundary:
Blank Boundary:
Boundary: Stock, Feedrate
Boundary members: Stock, Feedrate, Tool Position, User Defined Events (Post Commands)
Check Boundary:
Boundary: Stock
Boundary members: Stock
Planar Mill Operation Boundary:
Part Boundary:
Boundary: Stock, Feedrate
Boundary members: Stock, Feedrate, Tool Position, User Defined Events (Post Commands)
Blank Boundary:
Boundary: Stock, Feedrate
Boundary members: Stock, Feedrate, Tool Position, User Defined Events (Post Commands)
Check Boundary:
Boundary: Stock
Boundary members: Stock
Trim Boundary:
Boundary: Stock
ZLevel Mill Operation Boundary:
Trim Boundary:
Boundary: Stock
Area Mill Operation Boundary:
Trim Boundary:
Boundary: Stock
Data Members
has_stock
int
stock
double
has_feedrate
int
feedrate_unit
feedrate_value
double
has_tool_position
int
tool_position
Set to 1 if used, or else set to 0.